LTE FDD Signal Studio can support SIB transmission on DL-SCH with user defined SIB contents. This topic discusses how to setup up the SIB transmission measurement. Refer to 3GPP TS 36.321 and 3GPP TS 36.331.
User has generated their own SIB Contents.
This topic contains the following sections:
System Information Block (SIB): There are 13 SIBs (SIB1 to SIB13) in the above 3GPP standard specification. Each SIB contains specific information. SIB1 means System Information Block Type1.
System Information (SI): The System Information message is used to convey one or more System Information Blocks.
Assign SI message to SIBs combinations are flexibly defined in SIB1 contents.
SIB can be transmitted with following DCI combinations.
DCI Format | Resource Allocation Type |
---|---|
1A | Type 2, Localized |
1A | Type 2, Distributed |
1C | Type2, Distributed |
SIB1 is a special SIB which has a fixed schedule with a periodicity of 80 ms and repetitions made within 80 ms. The first transmission of SIB1 is scheduled in subframe #5 of the radio frames for which the SFN mod 8 = 0, and repetitions are scheduled in subframe #5 of all other radio frames for which SFN mod 2 = 0.
The SI messages are transmitted within periodically occurring time domain windows (referred to as SI-windows) using dynamic scheduling. Each SI message is associated with a SI-window and the SI-windows of different SI messages do not overlap. That is, within one SI-window only the corresponding SI is transmitted. The length of the SI-window is common for all SI messages, and is configurable. Within the SI-window, the corresponding SI message can be transmitted a number of times in any subframe other than the Multicast Broadcast Multimedia Services Single Frequency Network (MBSFN) subframes and subframe #5 of radio frames for which SFN mod 2 = 0. The UE acquires the detailed time-domain scheduling and other information (e.g. frequency-domain scheduling and used transport format) from decoding SI-RNTI on PDCCH (Refer to 3GPP TS 36.321).
SIB1 configures the SI-window length and the transmission periodicity for the SI messages.
SIB1 RV Index = ceiling (3/2*k) modulo 4, where k = (SFN/2) modulo 4.
SIB RV Index = ceiling (3/2*k) modulo 4, where k depends on the type of system information messages, k=i modulo 4, i =0,1,…, nsw–1, where i denotes the subframe number within the SI window nsw.
System Bandwidth = 10 MHz (50RB), SIB1 and SI1 (SIB2 and SIB3) message.
SIB1 is assigned to DL-SCH1
SI1 (SIB2 and SIB3) is assigned to DL-SCH2
SI-Window = 20 (ms)
User has generated their own SIB contents
Starting with the default setup for the N7624C Signal Studio software.
Delete the existing carrier.
Click Add Carrier and add
Carrier.At the Carrier node, in the
area, click and click on the down arrow to select . (Or in the node, you can click the button to access the same channel configurations.)Click
and set to .In the
node, select and then change to .Click
and set to 80 ms.Click DL-SCH1 Tx Sequence window.
to open theClick Column Preset button and select .
Click
to set the necessary state of the #5 of even number frame to on for the SIB transmission. (For this SIB1 transmission case, SIB1 transmission has to satisfy 3GPP section 5.2.1.2 of 36.331.)For this SIB Transmission example use the following settings:
Sequence # |
Frame #: |
Subframe # |
State |
---|---|---|---|
6 |
0 |
5 |
on |
26 |
2 |
5 |
on |
46 |
4 |
5 |
on |
66 |
6 |
5 |
on |
Click
and select , then enter 4 to satisfy TB #1 ≤ TB Size #1.Click
and select (default).Set each Subframe example is for SIB1 transmission.
(RV Index) using the values below. This
Sequence # |
Frame # |
Subframe # |
RV #1 (RV Index) Value |
---|---|---|---|
6 |
0 |
5 |
ceiling (3/2*(SFN/2) modulo 4) modulo 4 = 0 |
26 |
2 |
5 |
2 |
46 |
4 |
5 |
3 |
66 |
6 |
5 |
1 |
Refer to 3GPP section 5.3.1 36.321.
Click
to close DL-SCH1 Tx Sequence window.Click in the cell to open the Data Source Selection window and select . Then enter your own generated SIB contents by importing or direct entry into the bit field. Append zero bit (“0”) to make data length equal to the TB size set in step 6. Click when finished.
In the
node, select .In
, set to for SI1 (SIB2 and SIB3) message transmission.In the
, click the drop down and select .Click
and set to 80 ms.Click DL-SCH2 Tx Sequence window.
to open theClick
and click .Set the required Sequence 12, Frame 1, Subframe #1, check box.
of the Subframes to on for SI1 (for this example, SIB2 and SIB3) transmission. ClickFor this example of the SI1 message transmission case, it is assumed that the transmission on Sequence #12, Frame #1, Subframe #1 State = on. Transmission Sequence 12, Frame 1, Subframe #1 is just an example, you can select any subframe to transmit that satisfies the 3GPP standard. Refer to section 5.2.1.2 36.331.
Select MCS Index (MCS #1) to satisfy the desire TB Size ≤ setting TB Size.
Example: where 30 bytes (240 bits) = TB Size
Set
(MCS Index) to 8.Set
to 2 (default).Verify that TB Size now displays 256.
Set each Subframe RV #1 (RV Index).
For this example:
Sequence #12, Frame #1, Subframe #1 . (RV Index)= ceiling (3/2*(11 modulo 4)) modulo 4 = 1
Refer to 3GPP section 5.3.1 36.321.
Click
to close the DL-SCH2 Tx Sequence window.Generate user-defined SIB contents (customer supplied) and insert the data into
on DL-SCH2 as .Example where TB Size (User-Defined SIB Contents) < setting TB Size:
User-generated SIB contents is 240 bits
Setting TB Size is 256 bits
Set the data for
of DL-SCH2 as .Append 16 zero bit to user defined SIB contents.
Click
to close Data Source Selection window.